Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Infineon's Arduino-Compatible 24V PROFET Switch Shield Now at Mouser Electronics

October 27, 2016 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Protected Switch Shield with PROFET™ 24V for Arduino from Infineon Technologies. The Protected Switch Shield is a power switch evaluation board compatible with Arduino microcontroller boards and with Infineon's XMC™ microcontroller kits using the Arduino form factor.

The Infineon Protected Switch Shield, available from Mouser Electronics, allows engineers to quickly prototype and evaluate designs using the PROFET 24V family of protected MOSFETS. The shield is equipped with three protected high-side power MOSFETs — two BTT6030-2EKA and one BTT6020-1EKA — which offer a total of five 24V channels, each with a nominal current of 4A to 5A. PROFET intelligent power switches consist of DMOS power transistor and CMOS logic circuitry for complete built-in protection. The devices offer protection against overload, overvoltage, short-circuit, excessive temperature, loss of ground, power supply loss, and electrostatic discharge (ESD). The PROFET devices are also capable of protecting against dynamic overvoltage such as load dump and inductive load turn-off.

The shield runs off 8V - 36V nominal input voltage and provides a driver circuit with logic level inputs and load diagnosis with current sense capability. The PROFET 24V devices are designed to drive resistive, capacitive, and inductive loads such as automotive bulbs, valves, and supply switches for motors using PWM (up to 400 Hz) or DC.

To learn more, visit http://www.mouser.com/new/Infineon-Technologies/infineon-24v-shield-btt6030-shield/.


With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 600 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Infineon Technologies
Infineon Technologies is a leading global designer, manufacturer and supplier of a broad range of semiconductors used in various microelectronic applications. Infineon's product portfolio consists of logic products, including digital, mixed-signal, and analog integrated circuits, as well as discrete semiconductor products.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room