「讓創意化為現實」:

Engineering Big Ideas Logo

Intel’s history is replete with innovative firsts: the first EPROM, the first 8-bit microprocessor, the first MCU, the first single board computer, just to name a few. Even Moore’s Law, which essentially predicted the exponential rate of innovation in integrated circuit development, was first identified by Intel’s co-founder, Gordon Moore. As the company stands on the cusp of its second half century of innovation, its manufacturing and engineering expertise continues to produce products and technologies that are the foundation for advancements being made in areas like computer vision, artificial intelligence, quantum computing and so much more.

Harnessing silicon designed specifically for AI, end-to-end solutions that broadly span from the data center to the edge, and tools that enable customers to quickly deploy and scale up, Intel® AI is leading the next evolution of compute.

Intel® Neural Compute Stick 2

Intel® Neural Compute Stick 2 is powered by the Intel® Movidius™ X VPU to deliver industry leading performance, wattage, and power.

AAEON UP Squared AI Vision X Developer Kit

Kit allows for implementing computer vision solutions with support for deep learning inference across CPU, GPU, and VPU.

Intel® Optane™ technology provides an unparalleled combination of high throughput, low latency, high quality, and high endurance through a unique combination of 3D XPoint™ memory media, memory and storage controllers, IP interconnects, and software. Together, they deliver a revolutionary leap forward in decreasing latency for workloads demanding large capacity and fast storage.

Intel® Optane™ M10 Memory

Intel® Optane™ M10 Memory is a smart memory technology that accelerates a computer's responsiveness by accessing your most used applications and remembers them after powering down

Intel® Optane™ SSD 905p

Intel® Optane™ SSD 905p delivers breakthrough performance to meet demanding storage workloads in desktop or client workstations.

In today’s world, the number of connected devices and the amount of data continues to increase every day. The rate at which data arrives from these devices into data centers also continues to increase. By leveraging Intel® FPGAs as accelerators, a wide range of workloads can be enhanced to accommodate this increased data, and new demands for analyzing it.

Intel® Cyclone 10 FPGAs

The Cyclone® 10 device families support vertical migration and are optimized for high-bandwidth low-cost applications for smart, connected systems.

Intel® Enpirion® EN6338QI 3A PowerSoC

The EN6338QI integrates MOSFET switches, small-signal circuits, compensation, and the inductor in an advanced 3.75x3.75x1.9mm 19-pin aEASI package.

Episodes:

Bonus Features: