GaN HEMTs Power Electric Motor Reform
Image Source:
YAKOBCHUK VIACHESLAV/Shutterstock.com
By Steven Keeping for Mouser Electronics
Edited March 29, 2021 (Originally published October 10, 2018)
The demand for compact yet powerful electric motors brings new challenges for design engineers. To maximize power
output from smaller motors, engineers are turning to a high-voltage and high-frequency operation. Silicon
(Si) metal-oxide semiconductor field-effect transistors (MOSFETs) and integrated-gate bipolar transistors
(IGBTs)—upon which conventional switch-mode inverters (a vital element of modern electric motor controls) are based—are struggling to
cope with these operational demands. Limited power density and breakdown voltage thresholds restrict drive voltages,
and the rapid switching required for high-frequency operations pushes up power losses. The result is inefficiency
and heat buildup.
Gallium nitride (GaN) high electron mobility transistors (HEMTs) offer an alternative to MOSFETs and IGBTs for
high-voltage and high-frequency motor-drive applications. These wide bandgap (WBG) semiconductor devices are opening
up new applications for high-power density motors because they can handle higher voltages, currents, temperatures,
and switching frequencies with much lower losses than silicon transistors. The commercial availability of integrated
GaN HEMTs and driver inverter stages for high-power-density electric motor applications is easing the adoption of
the new technology.
GaN HEMT inverters complement a new generation of ceramic capacitors that can handle the high-voltage spikes and
surges that threaten to overstress conventional direct-current (DC) link components inherent to high-power-density
electric motors.
In the following, we’ll examine the challenges to components used in the power stages of high-power-density
electric motors and how GaN HEMTs and high-performance ceramic capacitors are proposed as a solution.
Advances in Electric Motor Design
Designers are demanding smaller, lighter electric motors that enhance existing products and enable use in a wide
range of new applications. High supply voltages and control frequencies promise a solution.
The Advantages of a High-Voltage Operation
Nominal motor power is the product of the supply voltage multiplied by current (V x A). Traditional electric motors
operate at low voltages (<1,000V), requiring them to run at high current to generate high power. The downside of
high-current operations is the need for larger coils, which increases coil resistance and lowers efficiency and
raises temperatures. High voltages (≥10kV) lowers current requirements allowing the use of smaller coils. The
downside is that the motor components (including the motor drive electronics) must handle the high voltages,
limiting options and increasing costs. A second downside is that small coils feature low inductance windings, which
are less able to damp the current ripple generated by switch-mode power supplies. Such a current ripple can lead to
electromagnetic interference (EMI) problems.
The Advantages of a High-Frequency Operation
A common type of modern motor is the three-phase alternating current (AC) type, driven by sequentially applying
current to each phase (winding) of the motor. The motor rotor is pulled around by the rotating magnetic field
generated by the windings, and its speed is proportional to the operating frequency
(Figure 1).
Figure 1: Sinusoidal signals applied to each phase of an induction electric
motor generate a rotating magnetic field that drags the rotor around. (Source: Sciencing)
Pulse-width modulation (PWM) is superimposed on the base operating frequency to control parameters such as start-up
current, torque, and power. The switching of semiconductor transistors (typically MOSFETs or IGBTs) determines the
PWM waveform.
A key advantage of high-frequency PWM is that current ripple—an artifact of the AC input after
rectification—is reduced, overcoming one drawback of smaller coils. Reduced current ripple requires smaller,
less expensive passive components for filtering. The high-frequency operation also reduces torque ripple—the
uneven electromotive force resulting from a less-than-perfect sinusoidal input to the motor coils—that can
cause motor vibration and premature wear.
Overall, high-frequency switching increases power density (power produced per unit volume), leading to smaller
motors with the same output as larger devices.
Conventional Motor Drives Reach Their Limits
Conventional three-phase AC motors run at voltages up to 1,000V and switching frequencies up to 20kHz. Such
operating parameters are well within the capabilities of inexpensive and commercially widespread silicon MOSFETs
used to construct the inverting bridges in the final stage of the motor drive.
However, silicon transistors reach their limits in high-power-density motor applications for these reasons.
- The components’ relatively low breakdown voltage limits supply voltages;
- The transistors’ switching losses—caused by residual resistance and capacitance every time the
transistor flips from on to off—rapidly outweighs efficiency gains as the operating frequency climbs;
- Because of a relatively long switching time, the devices reach a threshold beyond which a higher frequency
operation is not possible.
IGBTs’ higher breakdown voltage offers some respite, allowing engineers to increase operating voltages and
operating frequencies. But as the operating frequencies climb above 50kHz, the IGBTs begin to suffer from
unacceptable switching losses and can’t switch fast enough.
The GaN HEMT Advantage
Although silicon forms the mainstay of the electronics industry, other semiconductors are routinely used for
specialist applications demanding a high-voltage and high-frequency operation or needing a high-temperature
tolerance. These alternative semiconductors are characterized by a wide bandgap (WBG)—the measure of the
energy required to free an electron for conduction in a semiconductor—which markedly changes the electrical
properties of the material compared with silicon. WBG semiconductors have a bandgap of 2eV to 4eV compared with
silicon’s 1eV to 1.5eV. GaN is an example of a commercially available and proven WBG semiconductor.
Properties of WBGs
In silicon MOSFETs, temperatures above 100°C compromise controlled switching because some electrons gain enough
energy from the heat (rather than a switching voltage) to escape the parent atom. Because the electrons of a WBG
semiconductor require more energy to escape from an atom and contribute to conduction, the same effect doesn’t
occur in GaN transistors until the temperature reaches around 300°C.
WBG semiconductors exhibit a higher breakdown voltage (above 600V) than silicon. This is complex but is in part
because of a property called electron saturation velocity (also called electron mobility). The higher mobility
allows the WBG semiconductor material to handle twice the current density (A/cm2) of silicon. This
property also allows a GaN HEMT to switch in about one-quarter of the time it takes a silicon MOSFET to flip.
All semiconductor transistors exhibit an on-state power loss because of parasitic and electrode resistance. Other
factors such as inter-electrode capacitances also contribute to power losses. The losses occur every time a
transistor is switched and are proportional to the switching frequency and motor current. The parasitic and
electrode resistance of GaN HEMTs is about half that of a silicon MOSFET, and the inter-electrode capacitances are
about one-fifth. The difference dictates that GaN HEMT switching losses are around 10 percent to 30 percent of those
of a silicon MOSFET for a given switching frequency and motor current. IGBTs exhibit lower switching losses at high
frequencies than MOSFETs but are still much less efficient than GaN HEMTs.
A final advantage of GaN HEMTs is that the transistors don’t suffer from reverse-recovery charge—the
dissipation of minority carrier charge left over when a silicon MOSFET switches from on to off—which leads to
switch current overshoot (ringing) in silicon MOSFETs, potentially contributing to EMI.
The Use of GaN HEMTs in Electric Motor Design
The electrical properties of GaN HEMTs make them an attractive proposition for engineers designing compact,
high-voltage, and high-frequency electric motors. In summary, the devices offer the following upsides:
- High breakdown voltages, encouraging the use of higher (greater than 1,000V) input voltages
- High current densities, enabling GaN-based components to shrink with no reduction in power-handling
- Rapid switching capabilities, allowing a high-frequency (200kHz and above) electric motor operation
- High-frequency operation, limiting output current ripple and allowing a reduction in filter component size
- Low switching losses, limiting power dissipation, and improving efficiency
- High-temperature resistance, permitting the use of smaller heat sinks
- High-level integration, allowing GaN HEMTs to be fabricated on a chip (unlike silicon power components).
- Reduced bill of materials (BOMs) and solution sizes because in motor drive solutions, GaN HEMTs can handle
freewheeling current without the need of the antiparallel diodes required by IGBTs.
These advantages enable engineers to design highly compact motors with identical output to traditional motors that
are more than twice their size yet with much lower power consumption. The key downside is that GaN HEMT design
demands a high level of expertise in circuit development and testing.
Integrated Solutions Maximize GaN HEMT Benefits
Until recently, silicon MOSFETs and IGBTs retained one key advantage over GaN HEMTs—their widespread
commercial availability. But today, engineers have easy access to GaN HEMT technology. Even better, silicon vendors
now provide integrated solutions based on GaN HEMTs, simplifying a high-voltage and high-frequency AC motor inverter
stage.
Previously, the GaN HEMT was packaged as a discrete device with a separate driver because the transistors and
driver components were based on different process technologies and were often supplied by different manufacturers.
The downside of this arrangement was bond wires with parasitic resistance and inductance that added to switching
losses. Mounting the GaN HEMT and driver on the same lead frame eliminates common-source inductance, something
particularly important in fast-switching (high di/dt) circuits. Unwanted inductance generates ringing and can cause
current protection mechanisms to misbehave. A second key advantage of integrated packages: Thermal sensing can be
built into the driver, ensuring the shut-down of GaN HEMTs before damage occurs if an over-temperature situation
arises.
Texas Instruments offers a GaN HEMT and driver integration
in its LMG3410R070 GaN
power stage (Figure 2). The company describes this product as the industry’s first 600V GaN
driver product. The device is an 8mm x 8mm quad flat no-lead (QFN) multichip module (MCM), comprising a GaN HEMT and
driver with an integrated 20V series MOSFET. The on-resistance is a very low 75mΩ. The gate driver features a
built-in buck/boost converter to generate the negative voltage necessary to turn the GaN HEMT off.
Figure 2: Texas Instruments' LMG3410R70 GaN power stage integrates a GaN HEMT
and driver in a compact package. (Source: Texas Instruments)
A key advantage of the LMG3410 GaN power stage is its control over the slew rate during hard-switching. Such
control is important to limit printed circuit board (PCB) parasitic hindrances and EMI. This Texas Instruments
product uses a programmable current source to drive the GaN gate, enabling the slew rate to be set between 30V/ns to
100V/ns.
The LMG3410 also includes a useful fault output to inform the host microcontroller if switching stops because of a
fault event.
Two compact LMG3410 GaN power stages in a half-bridge configuration offer the rapid hard switching, low switching
loss, low parasitic inductance, and zero reverse-recovery charge that designers require to drive each phase of a
high-power-density electric motor (Figure 3).
Figure 3: This application circuit schematic shows two Texas Instruments GaN
power stages in a half-bridge configuration driving one phase of a three-phase motor. (Source: Texas
Instruments)
Building a Drive for High-Performance Electric Motors
A complete AC motor drive solution (Figure 4) comprises three elements: A rectifier (AC/DC
converter), a DC link, and an inverter (DC/AC converter).
Figure 4: This motor drive solution schematic illustrates a DC link
capacitor’s position. (Source: KEMET)
The rectifier, typically based on a diode or transistor topology, converts a standard 50 or 60Hz AC supply into an
(approximate) DC supply. DC power from the rectifier is filtered and stored in the DC link circuit until the
inverter uses it. The inverter then converts the DC supply into three sinusoidal PWM signals, each of which drives
one phase of the motor.
The DC element performs several key roles:
- Filtering of current and voltage ripple from the rectification stage
- Filtering of rectifier voltage transients that might otherwise damage the inverter’s transistors
- Improving circuit efficiency
- Limiting inductive currents that might otherwise damage the transistors
- Ensuring smooth power transfers to the loads
While a DC link circuit, comprising a single capacitor mounted across the power lines between the rectifier and
inverter stages of a motor drive, is simple to implement, its importance to the overall performance and efficiency
of the electric motor makes the selection of a quality component critical.
DC links operate in challenging conditions involving high-slew rates (dV/dt) and high-voltage peaks, so it is
important for a designer to select devices designed to withstand such stress. The KEMET KC-LINK capacitors—which use a
ceramic (calcium zirconate, CaO3Zr) dielectric along with nickel internal electrodes—are a good
option as they are purposely designed for high-voltage, high-frequency DC link applications.
Key attributes of the KC-LINK devices are the very low equivalent series resistances (ESRs) and equivalent series
inductances (ESLs). Low ESR and ESL values contribute to better efficiency, particularly in high-voltage
applications. In addition, the capacitors are able to operate at the high frequencies and high temperatures that are
common to next-generation electric motor applications. The capacitors can withstand frequencies up to 10MHz and a
temperature range from -55 to 150°C. The devices also feature no capacitive shifts with voltage changes, and
they are automotive qualified.
Conclusion
The commercial availability of WBG semiconductor devices such as GaN HEMTs for electric motor inverters and
high-performance capacitors for DC links is meeting the demand from designers for reliable components designed for
high-power-density electric motor drives. These key components will enable designers to enhance existing products
with compact, lighter, and less expensive motors while extending electric motor use to a wide range of new
applications. In addition, a new generation of high-power-density motors will significantly lower energy demands,
contributing to a greener planet.
Steven Keeping is a contributing writer
for Mouser Electronics and gained a BEng (Hons.) degree at Brighton University, U.K., before working in the
electronics divisions of Eurotherm and BOC for seven years. He then joined Electronic Production magazine and
subsequently spent 13 years in senior editorial and publishing roles on electronics manufacturing, test, and design
titles including What's New in Electronics and Australian Electronics Engineering for Trinity Mirror, CMP and RBI in
the U.K. and Australia. In 2006, Steven became a freelance journalist specializing in electronics. He is based in
Sydney.